This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK00804B-Q1: Reference voltage for LVDS signals

Guru 12365 points
Part Number: LMK00804B-Q1


Tool/software:

Hi,

We are considering a circuit that uses the LMK00804B-Q1 as a receiver to input an LVDS signal. In the circuit we are considering, we assume that the input signal to the LMK00804B-Q1 will be a differential signal with an amplitude of 188mV, but the reference voltage will be 0V. The reference voltage for a typical LVDS signal is thought to be 1.2V, so is it necessary to apply a 1.2V bias in an external circuit?

Thanks,

Conor