This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK05028: LMK05028

Part Number: LMK05028

Tool/software:

On the circuit, the 'LMK05028' and the oscillators (XO, TCXO) mentioned below are installed. Ref_IN1 is fed with 5MHz (LVCMOS).  We want to synchronize 125MHz (Out0) with REF_IN1.

Several tests were done by different threshold and LBW values and afterwards we looped back (5MHz) Out7 to REF_IN1, but DPLL1/2 did not lock. 

Test conditions:

 

TICS file:

LMK05028_SyncE.tcs

 

XO Oscillator:  48MHz  ±50ppm      (ECS-3225MV-480-BN) 

TCXO Oscillator:   19.2MHz  ±1ppm    (525L19210IT)

 

By programming the board with “LMK05028_SyncE.tcs” XO، TCXO and REF_IN1 deliver no fault.

Read Reg  0x0D  =  0x00          (XO and TCXO Validated)

Read Reg  0x2E6  =  0x20        (REF_IN1 Validated)

 

REF_IN1 Monitor mask register is as below:

Write Reg  0xBE  =  0x2F

 

Although APLL is locked, DPLL1/2 frequency and phases are not locked.

Read Reg  0x0D  =  0x00          (APLL 1/2 Locked)

Read Reg  0x0E  =  0xC0          (DPLL 1 Not Locked)

Read Reg  0x0F  =  0xC0          (DPLL 2 Not Locked)

My Schematic:LMK05028_SyncE.TCS