Part Number: LMK04808
Tool/software:
Hi Team,
For LMK04808, can I able to generate output clocks with connecting only OSCIN pins to a 20MHz oscillator (The CLKIN0 and CLKIN1 pins are NC)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: LMK04808
Tool/software:
Hi Team,
For LMK04808, can I able to generate output clocks with connecting only OSCIN pins to a 20MHz oscillator (The CLKIN0 and CLKIN1 pins are NC)?
Hi Sam,
Yes, that is possible. However, note that the mode of operation will only be single-loop. If you use one of the CLK inputs, you can jitter clean using the first loop. Otherwise, you will be able to use the 20 MHz input to generate the output frequencies you need using the VCO and the output dividers.
Thanks,
Michael