Other Parts Discussed in Thread: LMX2595,
Tool/software:
We are using the LMX2595 and LMX2820 synthesizers in our design and would like your clarification on the following SPI interface and logic level compatibility points:
-
LMX2595 – SPI with 1.8V Logic:
-
If we are using 1.8V logic for the SPI interface, do we need to connect any power input (such as VIO) externally to 1.8V to ensure proper logic level matching?
-
What logic level is supported on the MUXOUT pin in this case?
-
-
LMX2820 – SPI and Logic Level Considerations:
-
Does the LMX2820 require an external 1.8V supply to support 1.8V SPI logic?
-
We are planning to connect the SDI, SCLK, and CS pins to the 1.8V logic bank of the MCU, while connecting the MUXOUT (used for SPI readback) to a 3.3V logic domain.
-
Will this logic level mismatch cause any issue or damage?
-
Is there any provision or configuration available to make the MUXOUT pin output 1.8V logic to match the rest of the SPI lines?
-
-
-
General SPI Interface (for both parts):
-
Are there any recommended pull-up or pull-down resistors needed on the SPI lines?
-
Can the SPI bus be used in shared mode (multi-slave configuration) with other devices, and are there any precautions required for this?
-