This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMK5C33216EVM: No programed output signals

Part Number: LMK5C33216EVM
Other Parts Discussed in Thread: LMK5C33216

Tool/software:

Dear TI support team,
We are using a board LMK5C33216EVM
in our development process and TICSPro to program it. The board is running, and SPI communication is working; registers can be read and written. However, I'm currently not able to set any output signal. Regardless of the loaded configuration/registers, the scope is always showing only 125MHz on OU0 and 156.25MHz on OUT1, no output on others. I have read manuals from the website and also tried to load multiple config files from the TI forum, but the result is always the same.
No external reference, internal XO is ENA5591A 38.88MHz. In the first step, the board should produce output signals of different frequencies (for example, 10 MHz), just as a test. In the next step, it should accept a input signal (frequency or PPS) and reproduce the same output, shifted by a certain input value (in ns or ps).
Any help would be appreciated.