Hi Team,
Please let me ask you how to calculate the total current consumption (MAX) of LMK00306.
I am looking/reading the datasheet, page. 7 and page 25-26.
I am confused reading the description in page 25-26.
Below are the condition how our customer use LMK00306.
-----------------------------------------------------------------------------
- VCC is 3.3V
- VCCOA / VCCOB is 2.5V
- Input from CLKin0 and CLKin1 (CLKin selection)
- CLKoutAx : All 3 channel of Bank A are used in LVDS
- CLKoutBx : All 3 channel of Bank B are used in LVDS
- REFout : not used
-----------------------------------------------------------------------------
I have calculated the current consumption as follow, am I correct ?
ICC(MAX) = ICC_CORE(MAX) + ICC_LVDS(MAX) x 2 = 10.5 + 29.5 + 29.5 = 69.5mA
ICCO(MAX) = ICCO_LVDS(MAX) x 2 = 27.5 + 27.5 = 55mA
* I think ICCO_LVDS is the current consumption at VCCO=3.3V. But I believe current consumption at VCCO=2.5V should be lower than this value.
Best Regards,
Kawai