This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I want to integrate Z-comm CRO6835Z VCO with LMX2487EVM. As EVM has it's own VCO, and I intend to use both VCOs (on-board and external) for two different experiments, is there a way to integrate both VCOs with board and bypass one when the other is required?
Regards,
Nidhi Singh
Hi Nidhi,
The VCO can be replaced with a footprint compatible VCO. But there is no clean way to integrate both VCO at the same time on this board.
Do you need to experiment with both at the same time or one VCO at a time would be fine?
If you really need it, you might be able to add wires to the board and hack up the IF VCO.
To disable the VCO remove the resistors and drive the FinRF pin.
Best Regards,
Julian
If my post answers your question, please click on "Verify Answer" button below.