Dear Team,
We received the below customer questions regarding the CDCLVD2102 device.
Please advise.
Kind Regards,
Mo.
------
Dear Sir, I am facing a problem about some Clock Buffer device. The Part number: CDCLVD2102 The problem is about the EN pin.
On a state of Low input to it, we will receive STATIC "0".
1) Can you describe the Static Zero Output?
1.1) Will there be any leakage current on this state?
1.2) Is it a real ground state?
1.3) Describe as much the Voltage and Current of the outputs on the static 0 state. If you are familiar with any other clock buffer 1:1 (or more outputs) that has the ability to shut down the outputs (without any leakage current), please let me know.