Part Number: LMX2594
Other Parts Discussed in Thread: LMX2595
I need clarification on the Channel Divider frequency limitations shown in Table 8 of the data sheet. For dividers > 6 it states that the VCO must be kept below 10 GHz. But that introduces large gaps in the achievable output frequency range for some of the dividers . For example, how would an output at 900 MHz be produced? DIV 12 range ends at 833.333 MHz and DIV 8 begins at 937.5 MHz. I believe increasing the VCO limit to 11250 MHz allow all frequencies to be produced.