This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2531: Lock Detect Signal is Not Asserted in LMX2531.

Part Number: LMX2531
Other Parts Discussed in Thread: CODELOADER

I m programming LMX2531LQ1570E through an FPGA for 1600 MHz. I have composed  the registers values from codeloader software. But when I configure the LD pin as digital logic high or low it works but when i configure it for N/2 or R/2 it outputs incorrect values. When this pin is configured as digital lock detect then it never goes high. Kindly provide some suggestion that what could be the issue.