This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Accurate clock on an RS-485 long distance cable

Other Parts Discussed in Thread: ADS131E04, CDCE706, CDCM1802

Hello,

I need to distribute a very accurate clock signal to a remote device (maximum distance: about 50 meters) using RS485 physical standard.

The recipient clock must feed an ADS131E04 ADC, so its frequency should be 2.048 MHz.

I see that very accurate oscillators on the market only have outputs over 10 MHz, hence my idea is to use a 16.384 MHz oscillator and then use a frequency divider (counter?) in order to take it to 2.048 MHz, which should be low enough to go through the 50 meters cable with no problems.

Now my question is: I want to divide my accurate clock by 8 without losing accuracy; what is the best way to do that?

Is a counter the best device for me? Or should I choose a PLL based device (I used CDCE706 in the past...)? Or something else?

Thanks in advance.

Regards,

Stefano