Other Parts Discussed in Thread: TINA-TI, , TLC556, SN74LVC1G123
Tool/software: TINA-TI or Spice Models
I'm trying to simulate with part TLC556 and TLC552.
When I'm calculating the results myself with the provided formula's from the datasheet the results don't match.
I'm using the astable configuration
For example when simulating model TLC556 with the default provided values
Ra=2890Ohm
Rb= 11540Ohm
C1 =10nF
The title of the model states this should result in 10kHz
but when simulating I see ~8.5Khz (after removing the diode)
and when calculating the results using the datasheets formuals I get 5.55khz
Why do the results differ so much?
I'd like to use the TLC 552 (low supply voltage) in an ATE setup.
appreciate your feedback,
Kind regards,
Aart Nagelhout