Dears,
Our customer is using LMX2571 in his application. Now, he have a question about the output power of RFOUT_TX. The frequency of input signal is 13MHz, the output frequency is 72.1-75.44MHz. He want to get a 0 dBm output power, the configs of LMX2571 are as following : output type is Push-Pull, RFOUT_TX enable, RFOUT_RX disable, the low five bits of register of R24 and R8 are all 1. Does this configs could get a 0 dBm output power? If not, how to get a 0 dBm output power?
The customer detected the output power, it's about -3dBm, the input and output as follows:
Thanks for your help in advance.
Regards,
Ricardo