Part Number: CDCLVD1204
Other Parts Discussed in Thread: CDCLVD110A, , SN65LVDS2
Hello Experts,
There is a parameter of Vring, 10% max in CDCLVD1204 datasheet. Does Vring belong to any LVDS standard? I did not find this spec in CDCLVD110A datasheet.
Also, the frequency of CDCLVD1204 is 800MHz for differential inputs. What's the capacitive loading in this test? Some datasheet like SN65LVDS2 will explicitly specify 10pF as well as 100Ohms loading as the test conditions. However, I did not find the capacitive loading in the CDCLVD110A or CDCLVD1204 datasheet.