This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCI6214: CDCI6214 Crystal Question

Part Number: CDCI6214


HI there,

I have a question on the crystal requirements for the XO on the CDCI6214.

Customer wants to use ABM8W-25.0000MHZ-6-D1X-T3. If I look at the drive level of this crystal is 10uW typical and 100uW max. If I look at the CDCI6214 datasheet Pxtal shows a 100uW min. Do I assume that the drive level of the CDCI6214 will be at least 100uW and since this is the min value and the max value on the crystal, there is the chance that we could overdrive it? It looks we could drive it lower than a 100uW, so I just wanted to confirm that this crystal can or cannot be used with the CDCI6214. Thanks!