I have read the datesheet of LMK00101 and do not find the exact specification of the frequcency range of the input differential clock input CLKin0/CLKin0* and CLKin1/CLKin1*. In the following table extracted from the datasheet, although the frequcency range of OSC pins is specified, the frequcency range of CLKin0/CLKin0* and CLKin1/CLKin1* is not mentioned.
Can I have a 200MHz differential oscillator connected to CLKin0/CLKin0* and CLKin1/CLKin1*?