Part Number: LMX2594
Dear Sirs,
I've understood that the serial input signals of the LMX2594 are 1.8V compatible. This info is reported
in pag. 7 (SPI clock. High impedance CMOS input. 1.8-V to 3.3-V logic.) and pag. 11 (DIGITAL INTERFACE section)
of the datasheet.
I've understood also that the MUXout is not a 1.8V-logic compatible but only 3.3V-logic because the Voh min is Vcc-0.4 = 2.9.
Instead, the SYNC and SYSREFREQ input signals are defined CMOS and maybe 1.8V compatible reading
the pag. 11 (DIGITAL INTERFACE section) but in the pag. 7 is not defined 1.8-V to 3.3-V logic. Why?
The same problem there is for CE signal.
Could you help me to clear the different definitions?
Is it possible to drive the serial channel signals in 1.8V logic and the SYNC/SYSREFREF in 3.3V logic?
Thanks in advance.
Daniele Sassaroli