This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CDCE813-Q1: Less than 8kHz input

Part Number: CDCE813-Q1
Other Parts Discussed in Thread: CD74HC4046A, CD54HC297, CD54HC4046A

Hi team,

I would like to use this device to generate 24.576MHz clock from 8KHz reference clock.

It looks the minimum input clock frequency at PLL mode is 8MHz.

Is there other device that can achieve this function?

regards,