This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMX2594EVM: Voltage Drop between Supply Voltage and VCC

Part Number: LMX2594EVM

Hi,

I am working with the LMX2594EVM and am having trouble getting it to produce an output. I used a multimeter and measured the VCC voltage between VCC_TP and GND_TP on the board, and found that when I supply 3.3V at the VCC_SMA connector input, I am only getting 2.85V VCC. This is presumably below the minimum voltage required to drive the chip, so could explain why I am not getting any function from it. Upon start-up, with 3.3 V supply, I am drawing 0.14 A from my power supply.

If I apply small changes to the input voltage, I get a proportional linear change in VCC, which seems indicative of some voltage division, but inspection of the schematic doesn't show me where this voltage division may be. I'm not current limited in any way - it is set at 0.6 A per the user manual.

I am supplying my power from a DC power supply, using banana plugs, then into the DC input of a Bias-T. The RF input of the bias-T is open, and then the RF + DC output is connected to a coax-SMA cable to the VCC input port of the EVM.

Can anyone indicate whether this may be a problem with the board, or perhaps my method of supplying power? (I could not find much data online about providing power over coax - I'm unsure if there may be matching issues.)

Also, I'm quite tempted to just bump up my supply voltage to 3.8 V, expecting ~3.23 Vcc on the board, but I thought I should figure out a proper explanation first.

Regards.

Lawrence