Part Number: LMX2694-EP
Hi,
What is the optimum value of OUTx_PWR for 7.7 GHz output?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Please start with OUTx_PWR = 31 and adjust the register value as needed. The optimum power will depend on the pull-up component as well as the transmission line on the board so it is hard to recommend an optimal value. The best way to go about this is starting at 31 and experimenting with it.
Thanks,
Vibhu