Other Parts Discussed in Thread: CDCLVP1212,
Hello Team,
can you confirm/clarify the following point out of the table below:
- Is the RF input pin an I/O input? Or I/O input means only logic signal input?
- Before power supply(Vcc) turns on, is it possible to apply any signals into I/O pin? Because it beyond (Vcc (0V) + 0.3V) specification.
- If I have an RF signal on the input will I have problems
Same questions for the CDCLVP1212, if I have the RF signal and Vcc is 0V, do I have problems?
If there are problems we need to think about powering up the last device in the clock chain first and than one after the other till the RF source.
Thanks,
SunSet