Hi,
I am configuring the VCC of the CDCLVP1208 to operate at 3.3V, the input is ac coupled to a LVPECL oscillator that is operating at 2.5V VCC. The oscillator output level low is 1.095V and high is 1.475V, that yield a differential output voltage of 0.76Vp-p well within the CDCLVP1208's input range, 0.2 - 1.5V. I believe this configuration works fine, is there any other parameters that need consideration?
Thanks,
SB