I was really confused about the voltage level about C6678`s clock input. C6678 ` s data manual tells us that LJCB is ranged from -0.3V to 1.3V in table 6-1.but when I was reading "Clocking Design Guide for KeyStone Devices"--SPRABI4—November 2010, I can`t find the threshold limits about the LJCB in table 1, then I checked the whole table , I thought only HSTL standards could meet the requirements(-0.3 to 1.3V), because even the LVDS(1.8V) need 1.8V to identify VIH(min). Then In the EVM ,the chip CDCE62005 provide LVPECL/LVCMOS/LVDS output voltage level ,but does this meet the LJCB voltage range?
thanks!