Other Parts Discussed in Thread: CDCM6208
Hi,
I want to use my CDCM6208 board in order to output a clock signal from an external crystal input.
First, I tried to output a clock from the internal 30.72 MHz crystal and it worked as expected. Then, I removed the R72 and R73 resistors as explained in the EVM User's Guide and populated R87 with a connection.
This time, my board outputs different frequencies which have nothing to do with my input while my registers configuration should disable 7 of the 8 outputs.
Instead, these are the frequencies I measure in outputs : ~128 MHz on Y0/Y1, ~102 MHz on Y2/Y3, ~51 MHz on Y4/Y5 and ~26 MHz on Y6/Y7.
I also made sure my input signal was delivered by measuring it on the corresponding pin of the chip. My signal is a waveform of 10 MHz between -0.6 and 0.6 V (JMP11 on GND).
Is my signal voltage not high enough?
Does this correspond to the basic frequency configuration provided when there is a Loss Of Reference? I noticed it was the same frequencies we can find on the first two lines at page 38 of the CDCM6208 chip datasheet with a 1.2 factor (~26 x 1.2 = 30.72 ; ~52 x 1.2 = 61.44 ...).
Thanks you for your answers,
Simon