Part Number: DAC70501
Hi Team,
Currently, I used VDD=3.3V and set BUFF-GAIN=1, REF-DIV=0.
The configuration will trigger a reference alarm condition, we do see all the DAC outputs go to 0 V
Can we see normal Vout if VDD is changed to 5V and BUFF-GAIN=1, REF-DIV=0?
I know there is a headroom of VOUT, in our application, we only need VOUT max = 3V.
Thanks,
Hector