This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5675A: LVDS or LVPECL differential clock signals can be used for CLK/CLKC input?

Part Number: DAC5675A
Other Parts Discussed in Thread: CDCLVP1208

Hello,

Do customer uses LVDS or LVPECL differential clock signals for DAC5675A CLK/CLKC input?
Datasheet specifies |CLK-CLKC| min = 0.4V and |CLK-CLKC| min = 0.8V.
Usually, LVDS Vod minimum is around 0.25V, it less than the |CLK-CLKC| min.
And looking at TI LVPECL buffer CDCLVP1208 differential output level spec, Voou pp (min) is 0.65Vpp at 3.3V power supply. This means Vod(min) is 0.325V, less than the |CLK-CLKC| min too.
So, if DAC5675A |CLK-CLKC| min spec is true, it seems that it is difficult to support either LVDS or LVPECL clock input.

Best regards,

K.Hirano