Part Number: ADS1258
Other Parts Discussed in Thread: TMP235,
We have data acquisition boards each running 9 x ADS1258 in continuous conversion mode across 16 channels.
Our boards performed without issue for a few weeks running 24x7 at slightly elevated temperatures (50C) measured on the board using a TMP235 (internal temperature registers not tracked). One master ADS1258 per board runs an oscillator, the others take a clock signal from the master.
Our boards have become gradually less reliable. They refuse to initialise (SPI setting registers) unless they have been powered off for a few minutes. During running, from minutes to hours after power on, various ADS1258 fail to before others (not producing DRDY signals) until the master ADS1258 falls and the whole board fails to produce DRDY or respond to SPI.
Initially this seemed to be a temperature dependant issue but even running the boards at 20C in a climatic chamber, we are still seeing the issues.
Are there any known reliability issues of which we should be aware? Should we be using the ADS1258-EP instead?
We had of course initially assumed that the issue was with the power supply (each chip has an independent LDO providing clean power) or a manufacturing issue with our boards. However the issue is shared across boards and across various ADS1258 components so we are now starting to suspect these components.
Any insight would be appreciated - thanks.