This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1262: Fundamentals of Precision ADC Noise Analysis

Part Number: ADS1262


Hi TI Team,

   When I was going through "Fundamentals of Precision ADC Noise Analysis"(slyy 192).I couldn't understand how you calculated ENBW of Antialiasiing filter and Sinc4 filter(Chapter 2.2).

ENBW of Antialiasing Filter is 2.5khz,

ENBW of Sinc4 Filter is Infinity

and when we combine both 

ENBW is 14Hz.

As given in the document Pg26.

"Now that both filters are magnitude plots (in decibels [dB])with the same x-axis scale, you can simply add them together to determine the overall system ENBW."

Can anyone explain this.

Regards,

Venkatavel.

  • Hi Venkatavel,

    To combine the filters, both plots are simply added together point by point, as long as both plots are in dB.

    For this specific example, both sets of data were plotted in Excel and then added together to form the combined plot.

    -Bryan