Other Parts Discussed in Thread: ADC128S102EVM, LM4120
Hello - I am planning to use this component in a space application and would like to better understand what the recommend design guidance is for protecting the device during power-down.
I see on that datasheet that VD must be less than VA + 300mV, up to a maximum of 6.5V.
To power the ADC I have two separate 3.3V LDO's where VD is tuned to be slightly below VA, nominally. Additionally, these LDO's are sequenced during power-on such that VA always powers up first.
During power-down the design does not currently provide for any sequencing or other control to prevent VD from exceeding VA. What is the recommended design guidance in this case?
My initial assumption was that power sequencing or some other control is not necessary during power-down because there is not an active power source to drive current into the ADC to do damage. There is only the output capacitance of the LDO's (about 15uF each).
Would the TI engineering team provide further rationale on whether the above is appropriate?
Thank you,
Alex