This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1278EVM-PDK: Power down Error

Part Number: ADS1278EVM-PDK
Other Parts Discussed in Thread: ADCPRO, ADS1278

I have an ADS1278EVM-PDK Rev G and have been using it with ADCPro and the ADS1278EVM-PDK-SW software.

It has been working flawlessly up until now. I am able to establish a connection to the board and all channels switch on as they have done previously.

However, when I try to do anything after establishing the connection the following error message pops up:

An error occured with error code 6004
libmmb0.lvlib:check_styx_err.vi\<ERR>
cannot get a fid /ads1278evm/conf/powerdown

<b>Complete call chain:</b>
libmmb0.lvlib:check_styx_err.vi
libmmb0.lvlib:lvstyx_write_path.vi
libmmb0.lvlib:lvstyx_write_path_int.vi
ads1278evm.lvlib:ADS1278EVM.lvclass:ADS1278EVMPanel.vi:2

All jumpers are set to their default positions as per the User's guide. However, I have been using an external 5V reference voltage, hence switch S3 is set to Ext.