Other Parts Discussed in Thread: ADS1259, ADCPRO, ADS1282
I recently purchased the ADS1259 and ADS1282 evaulation kits and I am trying to talk to the ADS1259 via ADCPro. It appears to connect and download the firmware successfully. However, if I try to change a setting in the Labview interface I receive the following error:
An error occured with error code 6004
libmmb0.olvlib:check_styx_err.vi<ERR>
usb receive error /ads1259evm/ads1259/clk
<b>Complete call chain:</b>
libmmbo.lvlib:check_styx_err.vi
libmmb0.lvlib:lvstyx_read_all_path.vi
libmmb0.lvlib:lvstyx_read_all_path_bool.vi
ads1259evm.lvlib:ADS1259EVM.lvclass:ADS1259EVMPanel.vi:1
Before I received this error I had an error 85, but saw a similar post for the ADS1259, downloaded a new adcpro_evm.ini file and that error went away. I have tried to run ADCPro on both the MMB0 rev C board and MMB0 rec D board with the same error. I think that I have followed the jumper connections correctly. On the MMB0 board I have jumpered J12 and the +5V to +5VA. I have not jumpered +5V to +VA. The boot mode switch is set to USB. On the MMB0 board Ihave jumbered J12 and J13B; J13A is not jumpered.
I would appreciate any help that you can provide.
Best,
Scott