This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC39J84: No outputs and Lanes Errors for DAC39J84

Part Number: DAC39J84
Other Parts Discussed in Thread: LMK04828

Dear all,

I'm struggling with the configuration of the DAC39J84.

I do not see any outputs from the DAC due to errors on the lanes. Even if I'm able to  perform the NCO test and the PRBS test mode is successful. I kindly ask you if you can check the configuration of the DAC.

This is my configuration:

  • FMC120 from abaco DAC39J84 and LMK04828
  • Trenz board with TE0808 with 9EG.

On the FPGA side I'm usign the IP xilinx JESD204b (PG066) and IP JESD204 PHY (PG198).

I'm communicating with the DAC trough a I2C to SPI bridge.

Here is how the LMK is connected to the DAC and to FPGA and what the expected frequencies are  :

internal reference of the Board at 100 Mhz CLK2in input of LMK

DCLK0 → 1000 Mhz DAC clock

DCLK2 → 250 Mhz clock open in the design for debug

DCLK4 → 1000 Mhz ADC A clock

DCLK6 → 1000 Mhz ADC B clock

DCLK8 → 250 Mhz clock connected to the GTH Lines

DCLK10 → 250 Mhz clock connected to the GTH Lines

The configuration register are set as in the file lmk04828.txt.

LMK0482 configuration
0x0000   0x0010   
0x0002   0x0000   
0x0003   0x0006   
0x0004   0x00d0   
0x0005   0x005b   
0x0006   0x0020   
0x000c   0x0051   
0x000d   0x0004   
0x0100   0x0063   
0x0101   0x0022   
0x0102   0x0055   
0x0103   0x0005   
0x0104   0x0062   
0x0105   0x0000   
0x0106   0x0032   
0x0107   0x0055   
0x0108   0x006c   
0x0109   0x0022   
0x010a   0x0055  
0x010b   0x0005   
0x010c   0x0062   
0x010d   0x0000   
0x010e   0x0032   
0x010f   0x0011   
0x0110   0x0063   
0x0111   0x0022   
0x0112   0x0055   
0x0113   0x0005   
0x0114   0x0062   
0x0115   0x0000   
0x0116   0x0032   
0x0117   0x0055   
0x0118   0x0063   
0x0119   0x0022   
0x011a   0x0055   
0x011b   0x0005   
0x011c   0x0062   
0x011d   0x0000   
0x011e   0x0032   
0x011f   0x0057   
0x0120   0x006c   
0x0121   0x0022   
0x0122   0x0055   
0x0123   0x0005   
0x0124   0x0062   
0x0125   0x0000   
0x0126   0x0037   
0x0127   0x0001   
0x0128   0x006c   
0x0129   0x0022   
0x012a   0x0055   
0x012b   0x0005   
0x012c   0x0062   
0x012d   0x0000   
0x012e   0x0037   
0x012f   0x0001   
0x0130   0x0060   
0x0131   0x0022   
0x0132   0x0055   
0x0133   0x0005   
0x0134   0x0042   
0x0135   0x0000   
0x0136   0x00ff   
0x0137   0x0000   
0x0138   0x0020   
0x0139   0x0002   
0x013a   0x0006   
0x013b   0x0000   
0x013c   0x0000   
0x013d   0x0008   
0x013e   0x0002   
0x013f   0x0000   
0x0140   0x0000   
0x0141   0x0000   
0x0142   0x0000   
0x0143   0x0013   
0x0144   0x00ff   
0x0145   0x007f   
0x0146   0x0000   
0x0147   0x002c   
0x0148   0x0033   
0x0149   0x0000   
0x014a   0x0000   
0x014b   0x0020   
0x014c   0x00ff   
0x014d   0x0000   
0x014e   0x0000   
0x014f   0x007f   
0x0150   0x0000   
0x0151   0x0002   
0x0152   0x0000   
0x0153   0x0000   
0x0154   0x0078   
0x0155   0x0000   
0x0156   0x0000   
0x0157   0x0000   
0x0158   0x000a   
0x0159   0x0000   
0x015a   0x0032   
0x015b   0x00df   
0x015c   0x0020   
0x015d   0x0000   
0x015e   0x0000   
0x015f   0x000b   
0x0160   0x0000   
0x0161   0x0004   
0x0162   0x00d0   
0x0163   0x0000   
0x0164   0x0000   
0x0165   0x0004   
0x0166   0x0000   
0x0167   0x0000   
0x0168   0x0004   
0x0169   0x0049   
0x016a   0x0000   
0x016b   0x0020   
0x016c   0x0000   
0x016d   0x0000   
0x016e   0x0013   
0x0171   0x00aa   
0x0172   0x0002   
0x0173   0x0000   
0x0174   0x0000   
0x017c   0x0015   
0x017d   0x0033   
0x0182   0x0002   
0x0183   0x0002   
0x0184   0x00a0   
0x0185   0x0000   
0x0188   0x0000   
0x1ffd   0x0000   
0x1ffe   0x0000   
0x1fff   0x0000 

As it is possible to see form the configuration I'm programming the SYS REF as a gapped pulse.

For the DAC these are the main parameters:

L = 8

M = 4

F = 1

S = 1

HD = 1

Fdac = 1000 MHz

DACPLL enabled, VCO L-BAND P=4, M=2, N=2

JESD CLOCK DIVIDER 2

SERDES: 10 Gbps, Full Rate, PLL @ 2.5GHz, serdes_refclk_div=2, MPY =0b10100

Here the programming sequence

Operation Read/Write

Address

Value

Notes

HW DAC_RESET

(after applying this reset the DAC sif registers have the default values, so this hw reset is working)

Write

0x02

0x0082

Read

0x7F

0x800a

From data sheet versionid=0x1 from this register read is 0x2

write

0x1A

0x0

write

0x0

0x18

write

0x25

0x2000

JESDCLK_DIV

write

0x31

0x6C08

write

0x32

0x120

write

0x33

0xAF40

write

0x3B

0x8800

write

0x3C

0x828

write

0x3D

0x8E

write

0x3E

0x108

write

0x3F

0x0

write

0x46

0x44

write

0x47

0x190A

write

0x48

0x31C3

write

0x49

0x0

write

0x04

0xFF

Alarm MASK

write

0x05

0xC0F2

Alarm MASK

write

0x06

0xFF00

Alarm MASK

write

0x24

0x10

SYSREFMODE_for_clkdvr

write

0x1E

0x2222

set_SYSREF_for_DSP

write

0x1F

0x2220

set_SYSREF_for_DSP

write

0x20

0x2022

set_SYSREF_for_DSP

write

0x23

0x2022

set_SYSREF_for_DSP

write

0x5C

0x1111

SYSREFMODE_for_JESD

write

0x34

0x80

SYNC set the LVDS format

write

0x4B

0x1F00

Buffer=32 Frames = 1, Octets per frame = 1

write

0x4C

0x1F07

K=32,L=8

write

0x4D

0x0300

M = 3 S = 1

write

0x4E

0xF4F

SCR=0, High Density, N=16 N'=16

write

0x4F

0x1CC1

write

0x51

0xFF

write

0x52

0xFF

write

0x54

0xFF

write

0x55

0xFF

write

0x5F

0x123

write

0x60

0x4567

write

0x01

0x0000

write

0x03

0xA300

write

0x61

0x211

DAC_TX_EN

write

0x4A

0xFF1E

write

0x4A

0xFF1F

write

0x4A

0xFF01

Enable 1 PULSE on LMK04824

Clearing the config100-config107 (writing all 1 and then all zeros)

the lanes status registers config100-config107 gives 0x400

So we have a 'code synchronization error' and nothing from  the DAC outputs.

After the DAC programming sequence I can see that the SYNC signal after  toggling it stays high.

To see if I can obtain the output from the DAC and the SYSREF from the LMK, I tried to perform the NCO TEST and once I configured the output level from the SIF, the MIXER frequencies and send a SYSREF pulse I can obtain the sinusoids that I expect.

The other test I performed is the PRBS test by sending a PRBS sequence from FPGA and configuring the DAC lane by expecting the same PRBS or a different one.

The Alarm Pin goes high  when the DAC expecting a diffent sequence,  and it stays low when the PRBS sequence is correct. So from these test it looks like the SERDES link doesn't have any problems.

I also perform the link layer tests(about these tests I'm not completly sure about the programming sequence):

ILA test  from conf100-107 I obtain always 0x400 

K28.5 test: conf100-107 I obtain always 0x0 

D21.5 test : conf100-107 I obatin always 0x0

So apparently, the code synchronization error  seems to be the problem. 

Do you have any suggestions on how I can solve this problem?

Thanks for the attention

  • Dario,

    Why are you using the DACPLL? With your settings, this will be running at 1GHz with a 1GHz input reference clock. Not sure this is what you want. Based on all of your setting, this is what the DAC PLL output will be. If this is frequency you want, you will get better performance using the LMK clock as the DAC clock instead of the DAC PLL. 

    Regards,

    Jim 

  • Dear Jim,

    thank you for your reply. The configuration of the DAC has the main purpose of checking the input clock of the DAC. So it is just for debug.

    Now I configured the DAC to not use the DAC PLL, by doing some modifications on DAC registers:

    REG   VALUE

    0x1A    0x20

    0x31    0x1000

    0x32    0x0

    0x33    0x0

    But the conf100-107 give me 0x503. And the SYNC signal is just a pulse

    I tried to perform the PRBS test and the test is passed. But still, I'm not able to see any kind of output. 

    Thank you for your support

  • Dario,

    It appears you are not passing CGS. This is usually caused by a mismatch in clock frequencies between the receiver and transmitter. Please compare your DAC register settings with the one attached. With K =32, the max frequency you can use for SYSREF = 31.25MHz. SYSREF can be set to this value or this value divided by a whole integer. In the file attached, SYSREF = 7.8125MHz. This may be your issue.

    Regards,

    Jim

    1G_8411_K_32.cfg 

  • Jim, 

    I really thank you for your effort. I've checked all the registers and also the SYSREF clock as you suggested. I did not see any change in the outputs. And the SYNCb is a periodic square wave if the SYSREF is continuous. 

    Instead, when I use the DAC PLL at least I can see the SYNCb signal after toggling is going to be stable, as  I showed in the previous figure.

    The only way I was able to see something is to lower the lane rate from 10 Gbps to 5 Gbps. I supposed the motherboard doesn't support a high bit rate. So I did a new vivado design by setting the lane rate at 5 Gbps.

    -- after sending a SYSREF pulse I noticed a periodic behaviour on the SYNC signal

    and the DAC outputs were showing something 

    So as it is possible to observe both in Vivado and in the oscilloscope there is a periodic signal. So the oscilloscope was showing what the FPGA was sending. At this point, I activated my waveform generator on FPGA and I obtained what I expected. 

    I'm able to replicate this behaviour but I have to: activate the DAC PLL,  bypass the ILA sequence on the tx side and set the 0x4F register to 0x1CE1. The SYSREF is a pulse sequence at freq of 7.8125 MHz. I'm not able to replicate this at 10 Gbps.

    Do you have an opinion of what is happening? 

    Regards

    Dario

  • Dario,

    Some of the older Xilinx FPGA's with GTEX2 transceivers and -2 speed grade had a dead spot in the serdes that would not allow the part to work between 8-9.8Gsps. What device is the FPGA using? This issue may also be a limitation of the PCB you are using. 

    You may also be having issues with meeting SYSREF timing at higher sample rates. The two attached files will allow you test that the DAC clocking is working properly (NCO only test) and if SYSREF timing is meet.

    If you have access to the JTAG signals on the DAC, you could run an eye scan to observe the signal integrity of each lane. 

    Regards,

    Jim

     3566.DAC38J84 100MHz NCO Test.pptx7534.SYSREF trouble-shooting.docx