Part Number: DAC38RF82EVM
Other Parts Discussed in Thread: DAC38RF82, LMK04828
Hi,
I am starting to work with DAC38RF82EVM connected to KCU105 through FMC connector.
I am following 'slau711 - March 2017' document to have a working starting point.
I have followed sections 4, 6 & 7.6.2 (PLL mode of DAC38RF82EVM).
Everything seems ok, and I can do all configurations stated in such sections, but finally I am not getting the 1.9592 GHz signal.
The tool versions are:
- HSDC Pro: v5.2
- DAC38RF8x: v3p1 / build date: 04 February 2020
- Vivado: I have tried both 2016.3 and 2021.2
I have already checked the jumper settings of DAC38RF82EVM:
JP1: shunt 2-3
JP2: shunt 1-2
JP3/JP8/JP9/JP10/J11/J22: open
J23: shunt 1-2, 3-4, 5-6 7-8
What checks should I do to narrow the problem?
Thanks,
Miguel