Other Parts Discussed in Thread: ADS9120
I am having a really weird problem with ADS8411. I did project development with the device and had a working board. The analog and digital supplies were separate. At one point the device failed. I suspected it was because during power up I was exceeding the voltage difference between the to supply rails. I changed the design to where the two supplies are connected together. There now is only one +5V supply.
Since then I have replaced the part a number of times and have been unable to power it up. The device immediately overheats.
I noticed that one response listed this as a legacy device. Does this device have some kind of power up issue and is there a replacement?