We have a faulty lot of boards which have a high input current when Pin 9 and 10 are connected to +5V
The +VA pins are obviously not connected internally.
Which parts of the ADS8411 are supplied by Pin 9 and Pin 10
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
We have a faulty lot of boards which have a high input current when Pin 9 and 10 are connected to +5V
The +VA pins are obviously not connected internally.
Which parts of the ADS8411 are supplied by Pin 9 and Pin 10
Hello Martin,
Thank you for your post.
Given the age of this device, I don't have that information readily available. I'll see if someone can possibly look into the design. The suggested pin pairings for decoupling capacitors indicates that pins 9 and 10 may be used for different internal circuitry.
What is the magnitude of the current observed on each of those pins? Does it scale with sampling rate or input voltage?
Best regards,