This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: ads1299 precise sampling time

Part Number: ADS1299

Hi dear

We are using an ads1299 in our circuit and another part of our circuit is 16 LEDs switching 4Hz rate and after reading data we have a 4 Hz noise on power spectrum. I read entire datasheet and we just know the time of DRDY which data is ready to read on output. If I want to switch the LED exactly when the ads1299 is not sampling data from input pins, I should know when the ads1299 starts and stops sampling data.

in DR[2:0]=101 we know it takes 16393 tclk to prepare first data in output, and after that each tDR we have a new data, but I want to know where exactly data is sampled from input.

Thanks