I have designed an equipment where i use the DRDY pulse from the ADS1298 to trigger a sample of other devices.
However, I need to know if the sample that is ready for conversion, when the DRDY is triggered, is from that specific time or if their is a delay between conversion and when data is ready.
Perhaps the delay is specifically related to the t_settle time, Meaning that a sample rate of 1 kHz would have a delay of 4.5 ms relative to the DRDY.