Part Number: DAC38RF82EVM
Earlier this year I received help in the following thread where I needed help with synchronizing dac A and B on the DAC38RF82EVM.
I'm now returning to the project after some time and am finding the synchronization problem to be still present. I'm confused because I recall things working reliably last time and I am using the same provided configuration files and working with the same hardware.
Setup Description
TI Hardware
TSW14J56
DAC38RF82EVM
Configuration Files:
Config file provided by David C:
Initialization config file provided by Jim S:
/cfs-file/__key/communityserver-discussions-components-files/73/GUI-reset-no-LMK.cfg
Behavior:
The two DAC outputs will be synchronized about half of the time. Other times the outputs will be off by one or two samples typically.
There are errors that are reported whether or not the outputs are synchronized correctly
"DAC A, Lane 0 multiframe alignment error"
"DAC A, Lane 1 multiframe alignment error"
"DAC A, Lane 2 multiframe alignment error"
"DAC A, Lane 3 multiframe alignment error"
"DAC B, Lane 4 multiframe alignment error"
"DAC B, Lane 5 multiframe alignment error"
"DAC B, Lane 6 multiframe alignment error"
"DAC B, Lane 7 multiframe alignment error"
Questions:
I would appreciate some insight into how to debug this problem. Or please let me know if there are alternative register settings that would provide reliable synchronization.
Also I would appreciate some insight into the process of synchronizing the multi-DACs. Is it the same as multi-device synchronization between different discrete devices, with the use of SYSREF?