This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC38RF82EVM: Dual DAC, Real Mode, 4x interpolation, LMF=821 Synchronization between DACs

Part Number: DAC38RF82EVM
Other Parts Discussed in Thread: DAC38RF82, , DAC38J84

My intended application is to use the DAC38RF82 in dual dac mode with real inputs LMF=821 while using the onboard VCXO (CMODE4),  

I started with an example cfg file from another post.

8741.6144MSPS_8x_10M_ref_LMF_841.cfg

In the GUI I changed to 

Dual Dac

Real Input

4x Interpolation

This almost works. The correct signals are output but they do not reliably align in phase. Hitting the 'Reset DAC JESD Core & SYSREF TRIGGER' button will yield different phase alignments each time. Occasionally they will be phase aligned. The phase misalignment appears to manifest in discrete steps.

I presume that the problem has something to do with how the different DACs utilize SYSREF. I tried playing around with the JESD Block settings but did not have any success.

I would appreciate an example cfg for my application or guidance on how to modify the settings properly.