I am able to test clock modes other than 12b single CMODE5 successfully with the DAC38RF82EVM. The end use case for our project is single DAC, 2.66GSPS 12b, 1x interpolation, 4 lane. I have connected my clocks per the CMODE5 setup instructions - two signal generators with a common reference one to J4 and one to J1. I have tried setting the J4 reference to 1/4 of Fs (J1) and also to the frequency recommended by the HSDC GUI when the config is LMF=413. Neither setup shows an output to the spec-an. What other settings do I need to hit and what frequencies do I need to set my generators to? The manual is not clear.