This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1299: Does ADS1299 have the recommended sensor head.

Part Number: ADS1299


Dear Expert

TI ADS1299 is recommended to have the sensor head matching with the DEMO board, if yes, please recommend.

The main application of our project is the detection of attention or concentration of young children. It may take a long time to confirm the preliminary test, and the mass production is pending.

  • Hi Gabriel,

    Thanks for the support.

    There are many different kinds of wet or dry electrodes available in the market for EEG applications. However, we are not experts in the EEG electrode, so I do not have specific electrode recommendations for the intended application.

    Thanks

    -TC