Hi sir,
I have a question on the Data sheet of section '9.4.3.2 input signal step'.
https://www.ti.com/lit/ds/symlink/ads131e08s.pdf?ts=1637897228072&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FADS131E08S%253FkeyMatch%253DADS131E08SPAG%2526tisearch%253Dsearch-everything%2526usecase%253DOPN

the delay time is 4th according to the description.
If an external analog switch is used for ADS131E08S,
Does conversion time have some conditions?
For example, If I set DR[2:0]=001 32kSPS 16bit and get data only once in start, it is a timing diagram like the following.


For example, If I add AIN0 and AIN1 in the external in addition to AIN in this device in the following configuration,
is it possible to read the correct value when reading the timing as above?
(I am reviewing a total of 16CH sampling).

Thanks.
Regards,