Hi TI Expert,
I have a question about the VDD off-ramp requirement.
For some reason, we can meet the VDD off time and power on-ramp requirement, but we CANNOT meet VDD off-ramp.
Can we increase the VDD off time(maybe 2s or 3s) and skip the VDD off-ramp? The idea is to make sure that the POR capacitor is fully discharged enough before power up again.
From the following link, Page 2, it only says that "it is recommended to have a specified VDD off-ramp".
TI App. Note: http://www.ti.com/lit/an/sbaa161/sbaa161.pdf
From my perspective, it implies that maybe we don't need to meet VDD off-ramp in some cases. Please help to check on it.
Thank you so much.