This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TSW14J57EVM: Trigger Option of HSDC Pro for ADC12DJxx00RF_JMODE5

Part Number: TSW14J57EVM
Other Parts Discussed in Thread: ADC08DJ5200RFEVM, ADC12DJ3200EVM, ADC12DJ5200RFEVM

I'm using TSW14J57EVM Rev.E with ADC08DJ5200RFEVM.

The ADC EVM itself works with the setting of "ADC12DJxx00RF_JMODE5", but the Trigger Option of HSDC Pro is disabled at this setting.

Can I use external trigger mode with this boards?

I read the following Q&As. I guess it can be done by modifying ini file to use proper firmware and enable trigger option. 

TSW14J57EVM: Trigger Option of HSDC Pro for TSW14J57EVM + ADS54J66EVM - Data converters forum - Data converters - TI E2E support forums

TSW14J57EVM: Trigger Option - Data converters forum - Data converters - TI E2E support forums

  • Hi,

    Unfortunately, we don't have this option available for every FW and device using the TSW14J57EVM.

    I can double check to see what might be available. I will update you as soon as I hear back.

    Regards,

    Rob

  • User,

    There is one trigger mode we currently have working with the ADC12DJ3200EVM using mode 0. This is a 12 bit mode that would probably work with the ADC12DJ5200RFEVM but not the ADC0812DJ5200RFEVM as this only supports 8 bit mode. I am working with the software team to see if we can come up with an ini file that will work for you. This may not be available until early January due to the holiday break.

    Regards,

    Jim 

  • User,

    Please try the attached ini file for triggering with jmode5. You will need to place this file in the following folder on your PC and the re-launch HSDC Pro GUI:

    Trigger INI Target Location : C:\Program Files (x86)\Texas Instruments\High Speed Data Converter Pro\14J57revE Details\ADC files

    When opening HSDC Pro, this new ini option should be available in the device drop down window.

    Regards,

    Jim

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/73/ADC12DJxx00RF_5F00_JMODE5_5F00_trig.ini

  • Jim,

    Thanks for the quick response even if in holidays.

    I tried the attached ini file but the trigger seems not detected.

    I confirmed that ADC board works with "ADC12DJxx00RF_JMODE5", then, I selected "ADC12DJxx00RF_JMODE5_trig". The trigger options was enabled and I checked "trigger mode enabled". I applied 0-1.8V square wave to the TRIG_IN(J13), then, I pressed "Read DDR Memory". However, it says "No trigger occurred."

    I also tried software trigger generation, as Yasuhito mentioned in the previous Q&A. I connected TRIG_OUT_A(J14) and TRIG_IN(J13) and checked "Software Trigger Enable", then I clicked "Generate Trigger" button. However, it also failed with "No trigger occurred."

    Is there anything I missed to use trigger input?

    Regards,

    Hiroaki

  • User,

    Try using other firmware that is available with HSDC Pro. See attached.

    Regards,

    Jim

    trigger option with any of the below.docx  

  • Jim,

    "TSW14J57revE_16L_DDR_XCVR_FIRMWARE" and "TSW14J57RevE_16L_XCVR_ADCDDRDACBRAM" worked perfectly for me, but, "TSW14J57RevE_16L_XCVR_ADCBRAMDACDDR" was failed with "No trigger occurred."

    I share modified INI file that it automatically load proper firmware. 

    Thanks a lot.

    Hiroaki

    ADC12DJxx00RF_JMODE5_trig.zip