Hi Expert,
My customer have an issue that is not enough output amplitude with ADC09QJ1300EVM.
Test condition1 (no issue)
GUI : OnBoard 50M Ref, Fs=500Msps, JMODE10
RX_DIV = 16, 32 and 64
Output amplitude is 460mV @RX_DIV=16 (195.3MHz)
Output amplitude is 540mV @RX_DIV=32 (97.7MHz)
Output amplitude is 530mV @RX_DIV=64 (48.8MHz)
Test condition2 (issue)
GUI :OnBoard 50M Ref, Fs=800Msps, JMODE10
RX_DIV = 16, 32 and 64
Output amplitude is 280mV @RX_DIV=16 (312.5MHz)
Output amplitude is 380mV @RX_DIV=32 (156.25MHz)
Output amplitude is 340mV @RX_DIV=64 (78.125MHz)
*It is spec out V DIFF(min) 400m Vpp-DIFF
Also FPGA was not locked PLL at this test condition.
Measurement point
R234(DNP) J9 TRIGOUT+ side and R241(DNP) K9 RTIGOUT- side
Could you please give me your advice?
Thanks
Muk