Part Number: ADS1256
Hi team,
I would like to know if ADS1256 can reach 30KSPS when fCLKIN= 7.68MHZ and using single channel continuous acquisition?
If it can reach 30KSPS, the output data (30K × 24bit per second )of SPI interface are stable and up-to-date?
According to the datasheet table 15, when data rate = 30ksps, setting time = 5 DRDY periods, which implies that the maximum rate is less than 30ksps or not real-time data?
I want to fight out the meaning of table 15.

Best Regards,
Amy Luo