Part Number: TX517EVM
Other Parts Discussed in Thread: TX517,
Hi,
I measured OUTA and OUTB waveform according to advice, but could not get the waveform as shown in the datasheet.
connection setting:HV0:+1.9V,LV0:-1.9V,HV1:+15.0V,LV1:-5.2V,HV2:+8.0V,LV2:-3.0V,VDD:+5V,VEE:-5V,VAA:+2.5V,VCW=OPEN.
17level

32level

I confirmed the operation by measuring the waveform when the HV power supply was disconnected.
I do not think that destruction has occurred since each of the waveforms is showing.
HV1 pin of P1-Header open

HV2 pin of P1-Header open

HV2 and HV1 pin of P1-Header open

What is the cause of not getting waveforms as shown in the datasheet?
Best regards,