Part Number: AFE7225
The docs cover DFS_RX and DFS_TX which seem limited to LVDS-only (DFS_TX is in 5.7 - LVDX TX INPUT INTERFACE REGISTERS, and DFS_RX is in 5.8 - LVDS RX OUTPUT INTERFACE REGISTERS).
Is there a CMOS equivalent? The documentation is lacking on CMOS equivalents. For example, PATTERN_SEL_RX for LVDS is in Register 0x337 (again section 5.8). However, if you want the same feature in CMOS mode, you use register 0x031, which is exclusively documented in 11 - QUICK GUIDE and not in the register listing.
Are DFS_RX/DFS_TX applicable in CMOS? If not, is there a CMOS equivalent register?
Thanks!