Part Number: TSW14J57EVM
Good afternoon,
I create the frequency modulated signal in Python and save it to csv like in the image.

You can see that they are all sin signals with different frequencies.
However, when I loading it to the High Pro, sin signals are converted multiple rectangles, and amplitude is decreased as well by program.
As you can see all of them are simulated by rectangules, and amplitude is decreased from 32000 to 10.
Can you help me how I can solve this issue?
P.s: The way that I create the signal is like this
def sinusoid_generator(Amp,freq,t):
return Amp*np.sin(2*np.pi*freq*t)
t = np.linspace(0, 1, 65536)
saw_mod = np.array([])
for i in range(1,10):
saw_mod = np.concatenate((saw_mod,sinusoid_generator(32000,i,t)))