Hi,
In 1:2 Demux Non-DES Mode
CLK+/- (pin 18, and 19) is 250MHz, and
VINI+/-(pin 11 and 10) and VINQ+/-(pin 22 and 23) are active.
DCLK+/- is 125 MHz
Data is received on DI, and DId
Data is received on DQ, and DQd.
In the above scenario which is the first sample, Di or Did ? Similary DQ or DQd?
Thanks
Madhu